Post Go back to editing

How to keep galvanic isolation with in the system. LTC2984

PDFPDF

As per File: without spi isolator.pdf 

1) Use one DC-DC to generate  3.3V_AGND with ground labeled as AGND.

2) Use second DC-DC to generate  3.3V_DGND with ground labeled as DGND.

3) This configuration is simple and my component count is also less.

Now my question is that Is galvanic isolation present between Micro_controller and LTC2984?

As per File: with spi isolator.pdf 

1) Use one DC-DC to generate  3.3V_AGND with ground labeled as AGND.

2) Use second DC-DC to generate  3.3V_DGND with ground labeled as DGND.

3) In this place another component spi isolator for galvanic isolation

Now my question ..is first configuration ok? or I have to use second one ? My priority is galvanic isolation.

Parents
  • Hi

        The LTC2984 does not provide any isolation from the analog inputs to the digital. Therefore your first proposal does not provide galvanic isolation. Further, you will need to make sure you are using an isolating DC-DC converter topology.

        Take a look at the LTM2883  SPI isolator, it can isolate SPI from the microcontroller and also provide enough power to supply the LTC2984 on the isolated side. 

    -Logan

Reply
  • Hi

        The LTC2984 does not provide any isolation from the analog inputs to the digital. Therefore your first proposal does not provide galvanic isolation. Further, you will need to make sure you are using an isolating DC-DC converter topology.

        Take a look at the LTM2883  SPI isolator, it can isolate SPI from the microcontroller and also provide enough power to supply the LTC2984 on the isolated side. 

    -Logan

Children
No Data