Post Go back to editing

LT1025 to Compensate Multiple Thermocouples

My customer is looking for Thermocouple sensor solution

  • for the temperature sensing range, need to measure the temperature maximum degree is can up to 160degree. A typical normal value is 90~145 degree.
  • Need 5 channels

As mentioned, LT1025 able to compatible with Standard Thermocouples (E, J, K, R, S, T). 

LT1025 Operating temp – 55°C to 125°C

Can LT1025 still measure customer’s requested range 90-150°C?

If yes, I would like to propose LTK001 https://www.analog.com/media/en/technical-documentation/data-sheets/LTK001fa.pdf

Thanks.