Post Go back to editing

Question of ADATE209

Hi Sir,

1.According to ADATE209 datasheet Figure 13 CLC Disable and Enable, Showed CLC Enabled sign-wave amplitude small than Disabled, which result different than others.Is that correctly?

2. I can’t understand the Figure 14 chart, Are DROUT1 and DROUT2 differential output waveform? 

3. Since I still not clear VH/VL/VT performance, I would like to simulate ADATE209’s conduct before evaluate the demo board.

Could you help me to check the result as blow chart?

Condition: VH1=VH2=3V, VL1=VL2=2V, VT1=VT2=1V, TERM1=2V, DROUT will be amplitude VH – VL =1V. Vcom will equal to VT=1V.

Parents
  • Hi RayW,

    1. Thanks for pointing this one out. I think the line texture was mistakenly reversed. With CLC enabled, the output should have a larger swing since it is compensating for losses.

    2. DROUTx outputs are not differential. The figure is only showing the superimposed waveforms for transitions between VHx to VTx and between VLx to VTx.

    3. With regards to ADATE209 functionality, refer to the Logic Truth Table (Table 6 on page 15 of the datasheet). I'm pasting a snapshot below

Reply
  • Hi RayW,

    1. Thanks for pointing this one out. I think the line texture was mistakenly reversed. With CLC enabled, the output should have a larger swing since it is compensating for losses.

    2. DROUTx outputs are not differential. The figure is only showing the superimposed waveforms for transitions between VHx to VTx and between VLx to VTx.

    3. With regards to ADATE209 functionality, refer to the Logic Truth Table (Table 6 on page 15 of the datasheet). I'm pasting a snapshot below

Children