Post Go back to editing

AD7418 : OTI function

Hello,

I have a question from our customer about OTI function of AD7418.
He wants to use A1 input for this OTI function.
But it seems that the OTI only be function for channel 0 from data sheet.

In table-6 "AD7418 Pin Function Descriptions" , indicated as followings.

OTI : This is a logic output. The OTI is set if the result of a conversion on Channel 0 (temperature sensor) is greater than an 8-bit word in the TOTI setpoint register. The signal is reset at the end of a serial read operation.

" OTI only be function for channel 0. "

Is this recognition correct ?

Best regards,

ysuzuki

Parents
  • Hello Karen,

    Thank you for your support.

    > I understand they want to use an external temp sensor rather than the onboard sensor?

    Yes, the customer wants to use external temp sensor.

    I think that I introduce ADT7411 to the customer.

    It wiil need to change the thresihold by every INT event to make hysterisys.

    Best regards,

    ysuzuki

Reply
  • Hello Karen,

    Thank you for your support.

    > I understand they want to use an external temp sensor rather than the onboard sensor?

    Yes, the customer wants to use external temp sensor.

    I think that I introduce ADT7411 to the customer.

    It wiil need to change the thresihold by every INT event to make hysterisys.

    Best regards,

    ysuzuki

Children
No Data