Article What are the recommended configuration register settings for the MAX30003 in order to measure ECG?

A customer may use these MAX30003 register settings to measure ECG, but the settings should be modified according to the custom application. Note:  When working with the MAXREFDES100# Health Sensor Platform (HSP) and using the HSP tethered (USB cable connected), the third VCM lead for body bias must be used.

Here are the settings:

CNFG_GEN: 0x080000 This is for lead-off detection disabled. If you want lead-off detection enabled, see datasheet Table 21 for details.

CNFG_CAL: 0x000000 The calibration voltage should be disabled while measuring ECG.

CNFG_EMUX: 0x000000 Connect ECG leads, disconnect calibration voltages.

CNFG_ECG: 0x805000 128sps, DLPF and DHPF enabled.

CNFG_RTOR1: 0x3F6300 R-R enabled with default settings.

CNFG_RTOR2: 0x202400 default R-R settings.

SYNCH and FIFO_RST: set to 0x000000 to begin new ECG recording.

A similar post on mbed.org can be found here: https://os.mbed.com/questions/79566/The-best-configuration/ 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.