Article ADXL362: autosleep mode

Question

When I put the ADXL362 in Wake up or Measurement Mode it works fine. But when I
try AUTOSLEEP it doesn't work properly.

Answer

The autosleep configuration is active only if linked or loop modes are enabled.
On page 29 in table 13 are Bit Descriptions for ACT_INACT_CTL.
Bit 4 and bit 5 are for LINK/LOOP. It needs to be 01 for Linked Mode or 11 for
Loop Mode.

Two thoughts:
1. When you use the Autosleep function, the accelerometer basically
toggles between Wake-Up Mode and normal Measurement Mode based on absence or
presence of motion.

In the Wake-Up Mode, the Activity timer does not function; in other words, the
TIME_ACT setting is ignored, so it appears that the device is more sensitive to
disturbances.

2. When you use Autosleep, the part clears its own interrupt rather than
waiting for a microcontroller to clear it. It is possible that the perceived
increase in sensitivity is actually because the accelerometer spends more of
its time with a clear interrupt, in a state where it is capable of detecting
activity.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.