Article What is the series resistance of the CAL port in the MAX30009 and why is this important?

Please see image below. This shows one side of the MUX, the other side is identical. CAL1 and CAL4 have 176ohm + 100ohm= 276ohm series resistance whereas EL1 and EL4 have 30ohm + 17ohm = 47ohm series resistance which is much lower. This is important to note when using the calibration port as the same current and external load used when not calibrating might not exceed the compliance voltage, but when used for calibrating it may exceed it. The CAL port use should be limited to a current that does not hit the receive channel compliance threshold with a resistance load of (2*276) + Rcal.

 

For example: A current setting of 1.28mA RMS = 1.81mA peak = 3.62mApp. For EL1 and EL4, total resistance is 2*47 = 94 ohms * 3.62mApp = 340mVpp, which is under the compliance voltage. For CAL1 and CAL4, total resistance is 2*276 = 552 ohms * 3.62mApp = 1.998Vpp, which will definitely violate the compliance voltage. Please see the receive channel compliance voltage from the datasheet.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.