ADXRS610: FAQ

  • Created
  • Updated
Was this helpful?
  • ADXRS610: Calibration

    Question In the datasheet, it says:"Using a 3-point calibration technique, it is possible to calibrate the null and sensitivity drift of the ADXRS610 to anoverall accuracy of nearly 200°/hour. An overall…
  • ADXRS61x maximum range extension

    Question My customer has application using our products to measure rotate speed of motor. They change now to the new ADXRS610/613/614 devices. In my customer's old design, they could extend the measurement…
  • ADXRS61x range change similar to ADXRS300

    Question wants to expand the measurement range from 300°/s to 1200°/s. With the ADXRS300 it is possible by changing the value of an external resistor, can this technique also be used with ADXRS610…
  • Ultrasonic cleaning impact on iMems

    Question A customer used altra-sound(30w) to clean his PCB board of ADXRS610. He found that the output of the part is not correct after clean. As he said, there is no problem on his soldering and ESD…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.