ADXL345: FAQ

  • Created
  • Updated
Was this helpful?
  • ADXL345 - resonance frequency

    Question I checked the datasheet of the ADXl345 – I am missing the resonance frequency Answer It is 5500Hz like for the ADXL335!
  • ADXL345 EMC Tests for the ADXL345 at higher frequencies available?

    Question Are there any higher frequency EMC tests available for the ADXL345? Answer EMC testing has been performed for the 10 Hz – 1000 Hz but not at the 127.7 MHz frequency. These products are used…
  • ADXL345 ESD protection requirement

    Question How to add ESD protection diode to the ADXL345 Answer The ESD protection are needed for pin 1 (VDD I/O) and pin 6 (VS) on ADXL345. Just any ESD diode would work and serve the purpose of protection…
  • ADXL345 internal filter

    Question Could you give us some more detail of the ADXL345 insite Answer The internal filter is as follows: 1. There is a single pole analog anti-aliasing filter at ~1.6kHz. 2. The digital filter is…
  • ADXL345 Magnetic Interferance?

    Question I still wonder about whether the sensors fulfill the demands of the MRI environment? It has to withstand a static magnetic field of 3 Tesla (i.e. it should not contain any ferromagnetic materials…
  • ADXL345 over range shock recovery time

    Question How long does the ADXL345 take to recover from a high-shock overload before it starts to operate normally? Answer If accelerometers are exposed to stimulus above the rated range they simply…
  • ADXL345 performance in electro magnetic fields

    Question I want to use ADXL345 in airbone application and I am concerned about the performance in electro magnetic fields. But it seems there is no information about this in the datasheet. Answer The…
  • ADXL345 power consumption

    Question We use a ADXL345 in a product were we used to have a power consumption around 42µA. In the latest shipment of this product we use the same components and firmware but the power consumption…
  • ADXL345 range configuration

    Question I have some questions about the 0x31 DATA_FORMAT register of our ADXL345. If I set DATA_FORMAT = 0x00, make the Gee Range = +/-2g, then I can get 1g = 256 and this is reasonable (2^10/4g=256…
  • ADXL345 turn off Vs, while keeping Vddio powered, is this possible?

    Question ADXL345: Is it possible to turn off Vs, while keeping Vddio powered, to save power? Answer Yes but turning off Vs means reprogramming the entire part each time Vs is powerd-on. Standby mode…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.