ADXL203: FAQ

  • Created
  • Updated
Was this helpful?
  • Access to accelerometer's raw data

    Question I am currently working with a research lab on an inertial sensor, for the medical field. The sensor consists of several accelerometers (about twenty). Our results are very satisfactory, but…
  • ADXL: How do the different MEMs Accelerometer packages react to moisture?

    Question How do the different MEMs Accelerometer packages react to moisture? Answer Ceramic packages (like the ADXL203) are hermetic. The do not absorb or pass any moisture at all. Plastic packages …
  • ADXL203 vs ADXL204 at 3.3V

    Question How does the ADXL203 compare to the ADXL204, when powered with 3.3V? Answer The ADXL204 and the ADXL203 use the same silicon die. The difference is that the ADXL204 was trimmed AND tested at…
  • ADXL203/AD22037 Structure

    Question I would like to use a AD22037 accelerometer in a prototype, am I correct in assuming that it's a closed-loop pendulus accelerometer with capacitive pickoff? Answer The ADXL203/AD22037 are…
  • ADXL203: Measuring tilt angles

    Question In my project i want use accelerometer ADXL203 for measurement of the corner of the tilt. I interest what measure tilt corner each of axises to perpendicular planes of the Earth when accelerometer…
  • ADXL203: Self-test calibration

    Question We would like to use your ADXL203 like a tilt sensor in safety critical applications like platforms stability control (with humans on board). We MUST BE SURE that your ADXL203 works well without…
  • ADXL203CE containig iron?

    Question We have been asked by one of our customers to do acceleration tests on ADXL203CE Accelerometers for a space mission. In order to do test in the required axis, we need to place the components…
  • Inclinometer for marine use

    Question I manufacture very accurate 1-axis inclinometers for marine use and now one customer would like to add second axis to the inclinometer (not as accurate) a gyroscope (2/3-axis) and an accelerometer…
  • Q&A on ADXL203EB (Dual Axis Accelerometer Evaluation Board)

    Question 1. ADXL203 Accelerometer itself is marked 33878203xlI382, Is the accelerometer supposed to have a zero G bias of 0V or 2.5V? 2. At zero G upon measurement with an oscilloscope my accelerometer…
  • vibration sensors - recommendation

    Question I have been looking for some time to source a vibration sensor that I can mount on motors, etc, could you please tell me if you have any versions which produce a 0-10v or 4-10mA output or…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.