ADIS16209: FAQ

  • Created
  • Updated
Was this helpful?
  • ADIS16201 and ADIS16209 Pins 8 and 10 Grounded - Performance Issues

    Question I initially used the ADIS16201 in my design. I tied pins 8 and 10 to ground. Later, I redesigned my system and upgraded to the ADIS16209. Will ADIS16209 work even if pin 8 and 10 is connected…
  • ADIS16209 Datecode Revision Change

    Question What is the meaning of this „R“ in the Datecode 1224R of the ADIS16209. Answer The “R” indicates that these units have had the firmware upgrade, so they would behave the same way as units…
  • ADIS16209 self-test

    Question We have a problem with the self-test of ADIS16209 at power-on. Is it correct that there is a possibility to disable this function at the power-on setting the bit 10 in the register MSC_CTRL…
  • ADIS16209: How do I connect pins 7,8,10,11? There are contradictions in datasheet.

    Question There is some contradictory information in the ADiS16209 datasheet. While the pin configuration (Figure 5 ) states tha pins 7,8,10,11 are DNC (Do not connect), figure 23 shows a schematic…
  • ADIS16209: Stability and sensitivity

    Question For my application, timing is nearly no problem. I would rotate the sensor slowly (3 rev/min) around the axis which inclination should be determined. The measured acceleration shows a sine…
  • ADIS1620x Evaluation Board dimensions

    Question We designed a PCB and we want to mount ADIS16209 Evaluation Board on this PCB. Therefore the dimension of the board are important. This information is missing from the mechanical drawing in…
  • Bias Stability over 1 Year

    Question Do you have any aging data related to the one year bias stability? Answer The key limitation is in the ARW (Acceleration Random Walk). For the accelerometer in the ADIS16209, the ARW is ~30ug…
  • The direction of axis X and axis Y

    Question Below is the fig 18 in datasheet, I think, for the fig in the middle, it should be X out = 0, and Y out has a certain output; and the right fig has the same problem. It seems not correct of…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.