I have recently started working on setting up the Stingray platform on the ZCU102 board.
i followed up : https://wiki.analog.com/resources/eval/user-guides/x-band-platform hardware and software page.
ZCU102 is booting. USB to UART Bridge is working fine. I am able to SSH from another laptop over Ethernet as well.
Implemented the ADAR1000EVAL1Z Power Sequence.
When i had connected the XUD1a board over the second slot on the ZCU platform - the mxfe stopped lighting up on the boot.
after i performed ADXUD1AEBZ Interposer FMC EEPROM Programming, the MxFE board (ad9081) started powering on however, where I do "iio_info" - i can no longer see the ad9081 board. even with "iio_attr -D command" - it throw cant not find device.
i have attached 3 images - one just with AD9081 board to show that it shows up in iio_info. Then i plugged in Stingray - it doesn't show up. i finally conencted XUD1a also - it doesnt show up.