Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      By Kuo-Chang A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

EngineerZone
EngineerZone
Switches & Multiplexers
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Switches & Multiplexers
Switches & Multiplexers
Documents Where do I find the header files em_device.h, em_chip.h, em_cmu.h, em_emu.h, and em_gpio.h used in the EFM32 Platform firmware files for the MAXREFDES70?
  • Q&A
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • 1. Thermal Resistance Junction to Board (Theta JB): 2. Thermal Resistance Junction to Case (Theta JC):
  • +AD75019: FAQ
  • +AD8108: FAQ
  • +AD8111: FAQ
  • +AD8112: FAQ
  • +AD8113: FAQ
  • +AD8114: FAQ
  • +AD8117: FAQ
  • +AD8152 EVB: FAQ
  • +AD8156: FAQ
  • +AD8158ACPZ: FAQ
  • +AD8159: FAQ
  • +AD8174: FAQ
  • +AD8177: FAQ
  • +AD8185: FAQ
  • +AD8192: FAQ
  • +ADG1204: FAQ
  • +ADG1207: FAQ
  • adg1212: FAQ
  • +ADG1219: FAQ
  • +ADG1236: FAQ
  • +adg1404: FAQ
  • +ADG1409: FAQ
  • +ADG1421: FAQ
  • +ADG1434: FAQ
  • +ADG1436: FAQ
  • +ADG1604: FAQ
  • +ADG1606: FAQ
  • adg1608: FAQ
  • adg1611: FAQ
  • +ADG1612: FAQ
  • +adg201: FAQ
  • +ADG201ATQ: FAQ
  • +ADG2128: FAQ
  • +ADG3123: FAQ
  • +ADG3247: FAQ
  • +ADG3248: FAQ
  • +ADG324x: FAQ
  • +ADG3300: FAQ
  • +ADG3304: FAQ
  • +ADG3308: FAQ
  • +ADG330x: FAQ
  • +ADG333A: FAQ
  • +ADG406: FAQ
  • +ADG408: FAQ
  • +ADG409: FAQ
  • +ADG411: FAQ
  • +ADG412: FAQ
  • +ADG419: FAQ
  • +ADG426: FAQ
  • +ADG428: FAQ
  • +ADG438F: FAQ
  • +ADG442: FAQ
  • ADG451: FAQ
  • +ADG451BR: FAQ
  • +ADG452: FAQ
  • +ADG453: FAQ
  • +ADG4612: FAQ
  • +ADG465: FAQ
  • +ADG467: FAQ
  • ADG490: FAQ
  • +ADG506: FAQ
  • ADG508: FAQ
  • +ADG508A: FAQ
  • +ADG508AKN: FAQ
  • adg508f: FAQ
  • ADG508_thetaJC: FAQ
  • +ADG5204: FAQ
  • ADG5208: FAQ
  • +ADG5208F: FAQ
  • +ADG5248F: FAQ
  • +ADG52xxF: FAQ
  • +ADG5401F: FAQ
  • +ADG5404: FAQ
  • +ADG5413: FAQ
  • +ADG5436: FAQ
  • +ADG54xx: FAQ
  • +ADG54xxF: FAQ
  • +ADG601: FAQ
  • +ADG621: FAQ
  • +ADG623: FAQ
  • +ADG659: FAQ
  • +ADG701: FAQ
  • +ADG702: FAQ
  • +ADG706: FAQ
  • +ADG708: FAQ
  • +ADG709: FAQ
  • +ADG712: FAQ
  • +ADG715: FAQ
  • +ADG722: FAQ
  • +ADG728: FAQ
  • +ADG732: FAQ
  • +ADG733: FAQ
  • +ADG734: FAQ
  • +ADG741: FAQ
  • adg752: FAQ
  • +ADG772: FAQ
  • +adg779: FAQ
  • +ADG788: FAQ
  • +ADG801: FAQ
  • +ADG804: FAQ
  • +ADG819: FAQ
  • +ADG819BRM: FAQ
  • +ADG841: FAQ
  • +ADG884: FAQ
  • +ADG901: FAQ
  • +ADG936: FAQ
  • +ADGM1304: FAQ
  • +ADGS1408: FAQ
  • ADGS1412: FAQ
  • +ADN4600: FAQ
  • +ADN4604: FAQ
  • +ADN4605: FAQ
  • +ADN4612: FAQ
  • +ADV3200_3201: FAQ
  • +ADV3202_3203: FAQ
  • +ADV3224_3225: FAQ
  • +ADV3226: FAQ
  • +ADV3228_3229: FAQ
  • Analog Switch Training Videos
  • confusing redundant temperature spec info in datasheet
  • +DG201ADY+: FAQ
  • +DG300ABWE+: FAQ
  • +DG301ACWE+T: FAQ
  • +DG303AAK: FAQ
  • +DG303ABWE+: FAQ
  • +DG303ACWE: FAQ
  • +DG408DY+T: FAQ
  • +DG419DY+: FAQ
  • +DG419L: FAQ
  • +DG508ADJ+: FAQ
  • +DG509AAK/883B: FAQ
  • +DG509AAL/883B: FAQ
  • +DG509AAZ/883B: FAQ
  • +Digital Crosspoint Switch: FAQ
  • EVAL-ADG2128EBZ: FAQ
  • +HI-201HS: FAQ
  • Is it okay to connect the ADG1611BRUZ's and ADG1436YCPZ's Exposed Pad to Gnd?
  • Latch-up immune parts: FAQ
  • +Link to Switch and Multiplexer basics: FAQ
  • +Logic Drive: FAQ
  • +MAX14504: FAQ
  • +MAX14589E: FAQ
  • +MAX14589EEWL+: FAQ
  • MAX14661: FAQ
  • +MAX14661ETI+: FAQ
  • +MAX14662ETI+: FAQ
  • +MAX14724: FAQ
  • +MAX14756EUE+: FAQ
  • +MAX14759ETA+T: FAQ
  • +MAX14760ETA+: FAQ
  • +MAX14761ETA+T: FAQ
  • +MAX14762ETB+: FAQ
  • MAX14763ETA+: FAQ
  • +MAX14777GTP+: FAQ
  • MAX14778: FAQ
  • +MAX14778EETP+T: FAQ
  • +MAX14778ETP+: FAQ
  • +MAX14802CCM+: FAQ
  • +MAX14802ECM+: FAQ
  • +MAX14803AEWZ+: FAQ
  • +MAX14808ETK+: FAQ
  • +MAX14809ETK+: FAQ
  • +MAX14815EVKIT: FAQ
  • +MAX14866: FAQ
  • +MAX14866UTM+: FAQ
  • +MAX14895EETE+T: FAQ
  • MAX14983E: FAQ
  • +MAX14983EETJ+: FAQ
  • +MAX20086ATPA/VY+: FAQ
  • +MAX20087ATPA/VY+: FAQ
  • +MAX20327EWL+T: FAQ
  • +MAX30100: FAQ
  • MAX30105: FAQ
  • +MAX30105EFD+: FAQ
  • +MAX3079: FAQ
  • +MAX313FEPE+: FAQ
  • +MAX313LCSE+: FAQ
  • +MAX314LESE+: FAQ
  • +MAX3231E_BV_A1: FAQ
  • +MAX32565: FAQ
  • +MAX32600-J85A+: FAQ
  • +MAX32600-J85B+: FAQ
  • +MAX32600-KIT#: FAQ
  • +MAX32600-P85B+: FAQ
  • +MAX32600-W85B+: FAQ
  • MAX32600: FAQ
  • +MAX32600MBED#: FAQ
  • +MAX333AEUP+: FAQ
  • +MAX3378: FAQ
  • +MAX337EAI+: FAQ
  • +MAX3393: FAQ
  • -MAX3510: FAQ
    • Where do I find the header files em_device.h, em_chip.h, em_cmu.h, em_emu.h, and em_gpio.h used in the EFM32 Platform firmware files for the MAXREFDES70?
  • MAX3643: FAQ
  • +MAX3643ETG+: FAQ
  • +MAX3654ETE+: FAQ
  • +MAX3656ETG+: FAQ
  • +MAX3799: FAQ
  • +MAX3890: FAQ
  • +MAX393C/D: FAQ
  • +MAX393ESE+: FAQ
  • +MAX3942: FAQ
  • +MAX3945ETE+: FAQ
  • +MAX3948: FAQ
  • +MAX3949ETE+: FAQ
  • +MAX394EAP+: FAQ
  • +MAX3955ETJ+: FAQ
  • +MAX3967A: FAQ
  • +MAX3969: FAQ
  • +MAX3971A: FAQ
  • +MAX3984UTE+: FAQ
  • +MAX3996: FAQ
  • +MAX3997ETM+: FAQ
  • +MAX4051ACEE+: FAQ
  • +MAX4051ACSE+: FAQ
  • +MAX4051EEE+T: FAQ
  • +MAX4512: FAQ
  • +MAX4524LETB+: FAQ
  • +MAX4564: FAQ
  • +MAX4581: FAQ
  • +MAX4595: FAQ
  • +MAX4617EUE: FAQ
  • +MAX4622CPE+: FAQ
  • +MAX4635EUB+: FAQ
  • +MAX4638: FAQ
  • +MAX4639EGE+: FAQ
  • +MAX4644: FAQ
  • +MAX4656ESA+: FAQ
  • +MAX4662: FAQ
  • +MAX4684EBC_B1: FAQ
  • +MAX4702: FAQ
  • +MAX4704: FAQ
  • +MAX4708ESE+: FAQ
  • +MAX4730ELT+: FAQ
  • +MAX4733: FAQ
  • MAX4781: FAQ
  • +MAX4781EGE+: FAQ
  • MAX4782: FAQ
  • +MAX4782ETE+: FAQ
  • +MAX4800ACCM+: FAQ
  • +MAX4890EETJ+: FAQ
  • +MAX4891ETJ: FAQ
  • +MAX4892EETX+: FAQ
  • +MAX4937CTN+: FAQ
  • +MAX4940ETL+: FAQ
  • +MAX4948ETG+: FAQ
  • +MAX4968: FAQ
  • +MAX4999: FAQ
  • +MAX4999ETJ+: FAQ
  • +MAX7356: FAQ
  • +MAX7357: FAQ
  • +MAX7358ETG+: FAQ
  • +MEMS Switch Technology: FAQ
  • Multiplexer Settling Time
  • Multiplexor and switch noise specifications
  • +Precision Technology Learning Modules
  • +SW02: FAQ
  • +SW06: FAQ
  • +Switch & Multiplexer: FAQ
  • +Switches and Multiplexers: FAQ
  • Theta JA(Junction to Ambient Temperature) and Theta JC (Junction to case Temperature)
  • What is the role of the Control Echo Enable bit?

Where do I find the header files em_device.h, em_chip.h, em_cmu.h, em_emu.h, and em_gpio.h used in the EFM32 Platform firmware files for the MAXREFDES70?

These resources come from Silicon Labs rather than Maxim.  These header files are apart of the emlib, which is standard across all the EFM32 devices.  For more information on this, please see the following link for the EFM32 Zero Gecko Software Documentation : http://devtools.silabs.com/dl/documentation/doxygen/5.7/efm32zg/html/index.html

Tags: emlib MAXREFDES50 MAX3510 EFM32 KA-09533