Yes. The MAX30105 has an on chip temperature sensor for calibrating the temperature dependence of the particle sensing sub-system, and so is cabable of giving a temperature reading with a resolution of 0.0625°C. It is the software that controls when the temperature data registers are read by the processor. Maxim supports only the physical layer. The software depends on the customer themselves or our algorithm partner: Valor Fire Safety, LLC (“Valor”).
Contact Valor for licensing information at www.valorfiresafety.com/licensing/