Question
I need more information about the digital Supply Voltage of the AD8112.
Which is the operating voltage of the digital part?
Can I use a 3.3 volt digital power supply?
If the the analog supply is +-5Volt and the digital supply is +5V, can I drive
the device with a microcontroller that working at 3.3?
Answer
The digital supply for the AD8112 is specified with -4.5V - +5V. This means you
cannot supply with 3.3V
The device works on 5V Logic.
High is specified: >=2.4V
Low is specified
If your microcontroller is capable (and specified) to deliver a High Signal
>2.4V and a Low Signal < 0.4V it might work. - this is depending on the uC
capabilities.
An alternative could be a level converter like the ADG3123 (to be on the safe
side)
http://www.analog.com/en/interface-isolation/level-translators/adg3123/products/
product.html
You can find all level translators here:
http://www.analog.com/en/interface-isolation/level-translators/products/index.ht
ml