Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Fast-Track Certification: Leveraging IC Safety App Notes for Functional Safety Designs
    View All Webinars
  • Community Hub

    Challenge Yourself!

      World Engineering Day Quiz!

      By Kuo-Chang A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

EngineerZone
EngineerZone
Switches & Multiplexers
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Switches & Multiplexers
Switches & Multiplexers
Documents What happens if the serial interface lines are active when Vcc not connected?
  • Q&A
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • 1. Thermal Resistance Junction to Board (Theta JB): 2. Thermal Resistance Junction to Case (Theta JC):
  • +AD75019: FAQ
  • +AD8108: FAQ
  • +AD8111: FAQ
  • +AD8112: FAQ
  • +AD8113: FAQ
  • +AD8114: FAQ
  • +AD8117: FAQ
  • +AD8152 EVB: FAQ
  • +AD8156: FAQ
  • +AD8158ACPZ: FAQ
  • +AD8159: FAQ
  • +AD8174: FAQ
  • +AD8177: FAQ
  • +AD8185: FAQ
  • +AD8192: FAQ
  • +ADG1204: FAQ
  • +ADG1207: FAQ
  • adg1212: FAQ
  • +ADG1219: FAQ
  • +ADG1236: FAQ
  • +adg1404: FAQ
  • +ADG1409: FAQ
  • +ADG1421: FAQ
  • +ADG1434: FAQ
  • +ADG1436: FAQ
  • +ADG1604: FAQ
  • +ADG1606: FAQ
  • adg1608: FAQ
  • adg1611: FAQ
  • +ADG1612: FAQ
  • +adg201: FAQ
  • +ADG201ATQ: FAQ
  • +ADG2128: FAQ
  • +ADG3123: FAQ
  • +ADG3247: FAQ
  • +ADG3248: FAQ
  • +ADG324x: FAQ
  • +ADG3300: FAQ
  • +ADG3304: FAQ
  • +ADG3308: FAQ
  • +ADG330x: FAQ
  • +ADG333A: FAQ
  • +ADG406: FAQ
  • +ADG408: FAQ
  • +ADG409: FAQ
  • +ADG411: FAQ
  • +ADG412: FAQ
  • +ADG419: FAQ
  • +ADG426: FAQ
  • +ADG428: FAQ
  • +ADG438F: FAQ
  • +ADG442: FAQ
  • ADG451: FAQ
  • +ADG451BR: FAQ
  • +ADG452: FAQ
  • +ADG453: FAQ
  • +ADG4612: FAQ
  • +ADG465: FAQ
  • +ADG467: FAQ
  • ADG490: FAQ
  • +ADG506: FAQ
  • ADG508: FAQ
  • +ADG508A: FAQ
  • +ADG508AKN: FAQ
  • adg508f: FAQ
  • ADG508_thetaJC: FAQ
  • +ADG5204: FAQ
  • ADG5208: FAQ
  • +ADG5208F: FAQ
  • +ADG5248F: FAQ
  • +ADG52xxF: FAQ
  • +ADG5401F: FAQ
  • +ADG5404: FAQ
  • +ADG5413: FAQ
  • +ADG5436: FAQ
  • +ADG54xx: FAQ
  • +ADG54xxF: FAQ
  • +ADG601: FAQ
  • +ADG621: FAQ
  • +ADG623: FAQ
  • +ADG659: FAQ
  • +ADG701: FAQ
  • +ADG702: FAQ
  • +ADG706: FAQ
  • +ADG708: FAQ
  • +ADG709: FAQ
  • +ADG712: FAQ
  • +ADG715: FAQ
  • +ADG722: FAQ
  • +ADG728: FAQ
  • +ADG732: FAQ
  • +ADG733: FAQ
  • +ADG734: FAQ
  • +ADG741: FAQ
  • adg752: FAQ
  • +ADG772: FAQ
  • +adg779: FAQ
  • +ADG788: FAQ
  • +ADG801: FAQ
  • +ADG804: FAQ
  • +ADG819: FAQ
  • +ADG819BRM: FAQ
  • +ADG841: FAQ
  • +ADG884: FAQ
  • +ADG901: FAQ
  • +ADG936: FAQ
  • +ADGM1304: FAQ
  • +ADGS1408: FAQ
  • ADGS1412: FAQ
  • +ADN4600: FAQ
  • +ADN4604: FAQ
  • +ADN4605: FAQ
  • +ADN4612: FAQ
  • +ADV3200_3201: FAQ
  • +ADV3202_3203: FAQ
  • +ADV3224_3225: FAQ
  • +ADV3226: FAQ
  • +ADV3228_3229: FAQ
  • Analog Switch Training Videos
  • confusing redundant temperature spec info in datasheet
  • +DG201ADY+: FAQ
  • +DG300ABWE+: FAQ
  • +DG301ACWE+T: FAQ
  • +DG303AAK: FAQ
  • +DG303ABWE+: FAQ
  • +DG303ACWE: FAQ
  • +DG408DY+T: FAQ
  • +DG419DY+: FAQ
  • +DG419L: FAQ
  • +DG508ADJ+: FAQ
  • +DG509AAK/883B: FAQ
  • +DG509AAL/883B: FAQ
  • +DG509AAZ/883B: FAQ
  • +Digital Crosspoint Switch: FAQ
  • EVAL-ADG2128EBZ: FAQ
  • +HI-201HS: FAQ
  • Is it okay to connect the ADG1611BRUZ's and ADG1436YCPZ's Exposed Pad to Gnd?
  • Latch-up immune parts: FAQ
  • +Link to Switch and Multiplexer basics: FAQ
  • +Logic Drive: FAQ
  • +MAX14504: FAQ
  • +MAX14589E: FAQ
  • +MAX14589EEWL+: FAQ
  • MAX14661: FAQ
  • +MAX14661ETI+: FAQ
  • -MAX14662ETI+: FAQ
    • Can the MAX14662 withstand +/-5.5V on the input and output pins while unpowered?
    • MAX14662 internal charge pump frequency
    • What happens if the serial interface lines are active when Vcc not connected?
    • What is the input and output capacitance for the ON and OFF states of the MAX14662 Octal Analog Switch?
    • What is the polarity (CPOL) and phase (CPHA) of the SPI interface in the MAX14662?
  • +MAX14724: FAQ
  • +MAX14756EUE+: FAQ
  • +MAX14759ETA+T: FAQ
  • +MAX14760ETA+: FAQ
  • +MAX14761ETA+T: FAQ
  • +MAX14762ETB+: FAQ
  • MAX14763ETA+: FAQ
  • +MAX14777GTP+: FAQ
  • MAX14778: FAQ
  • +MAX14778EETP+T: FAQ
  • +MAX14778ETP+: FAQ
  • +MAX14802CCM+: FAQ
  • +MAX14802ECM+: FAQ
  • +MAX14803AEWZ+: FAQ
  • +MAX14808ETK+: FAQ
  • +MAX14809ETK+: FAQ
  • +MAX14815EVKIT: FAQ
  • +MAX14866: FAQ
  • +MAX14866UTM+: FAQ
  • +MAX14895EETE+T: FAQ
  • MAX14983E: FAQ
  • +MAX14983EETJ+: FAQ
  • +MAX20086ATPA/VY+: FAQ
  • +MAX20087ATPA/VY+: FAQ
  • +MAX20327EWL+T: FAQ
  • +MAX30100: FAQ
  • MAX30105: FAQ
  • +MAX30105EFD+: FAQ
  • +MAX3079: FAQ
  • +MAX313FEPE+: FAQ
  • +MAX313LCSE+: FAQ
  • +MAX314LESE+: FAQ
  • +MAX3231E_BV_A1: FAQ
  • +MAX32565: FAQ
  • +MAX32600-J85A+: FAQ
  • +MAX32600-J85B+: FAQ
  • +MAX32600-KIT#: FAQ
  • +MAX32600-P85B+: FAQ
  • +MAX32600-W85B+: FAQ
  • MAX32600: FAQ
  • +MAX32600MBED#: FAQ
  • +MAX333AEUP+: FAQ
  • +MAX3378: FAQ
  • +MAX337EAI+: FAQ
  • +MAX3393: FAQ
  • +MAX3510: FAQ
  • MAX3643: FAQ
  • +MAX3643ETG+: FAQ
  • +MAX3654ETE+: FAQ
  • +MAX3656ETG+: FAQ
  • +MAX3799: FAQ
  • +MAX3890: FAQ
  • +MAX393C/D: FAQ
  • +MAX393ESE+: FAQ
  • +MAX3942: FAQ
  • +MAX3945ETE+: FAQ
  • +MAX3948: FAQ
  • +MAX3949ETE+: FAQ
  • +MAX394EAP+: FAQ
  • +MAX3955ETJ+: FAQ
  • +MAX3967A: FAQ
  • +MAX3969: FAQ
  • +MAX3971A: FAQ
  • +MAX3984UTE+: FAQ
  • +MAX3996: FAQ
  • +MAX3997ETM+: FAQ
  • +MAX4051ACEE+: FAQ
  • +MAX4051ACSE+: FAQ
  • +MAX4051EEE+T: FAQ
  • +MAX4512: FAQ
  • +MAX4524LETB+: FAQ
  • +MAX4564: FAQ
  • +MAX4581: FAQ
  • +MAX4595: FAQ
  • +MAX4617EUE: FAQ
  • +MAX4622CPE+: FAQ
  • +MAX4635EUB+: FAQ
  • +MAX4638: FAQ
  • +MAX4639EGE+: FAQ
  • +MAX4644: FAQ
  • +MAX4656ESA+: FAQ
  • +MAX4662: FAQ
  • +MAX4684EBC_B1: FAQ
  • +MAX4702: FAQ
  • +MAX4704: FAQ
  • +MAX4708ESE+: FAQ
  • +MAX4730ELT+: FAQ
  • +MAX4733: FAQ
  • MAX4781: FAQ
  • +MAX4781EGE+: FAQ
  • MAX4782: FAQ
  • +MAX4782ETE+: FAQ
  • +MAX4800ACCM+: FAQ
  • +MAX4890EETJ+: FAQ
  • +MAX4891ETJ: FAQ
  • +MAX4892EETX+: FAQ
  • +MAX4937CTN+: FAQ
  • +MAX4940ETL+: FAQ
  • +MAX4948ETG+: FAQ
  • +MAX4968: FAQ
  • +MAX4999: FAQ
  • +MAX4999ETJ+: FAQ
  • +MAX7356: FAQ
  • +MAX7357: FAQ
  • +MAX7358ETG+: FAQ
  • +MEMS Switch Technology: FAQ
  • Multiplexer Settling Time
  • Multiplexor and switch noise specifications
  • +Precision Technology Learning Modules
  • +SW02: FAQ
  • +SW06: FAQ
  • +Switch & Multiplexer: FAQ
  • +Switches and Multiplexers: FAQ
  • Theta JA(Junction to Ambient Temperature) and Theta JC (Junction to case Temperature)
  • What is the role of the Control Echo Enable bit?

What happens if the serial interface lines are active when Vcc not connected?

The MAX14662 is able to withstand voltages from -0.3V to 6V on the serial interface lines (i.e. /CS/AD0, DOUT/AD1, SCLK/SCL, DIN/SDA). As long as the signals are within this range the device will not become damaged. The serial interface engine is not active when Vcc is not connected. Please reference the "Absolute Maximum Ratings" section to ensure these specifications are not violated.
Tags: MAX14662ETI+ 000097399 Analog Switches Multiplexers switches and multiplexers MAX14662