The MAX14724 is a matrix MUX. This means that each input can be connected to any output. This is a cross point switch. The MAX14724 is also a passive MUX. This means that the input and the output are not isolated. Therefore, you should keep isolation in mind if you are intending to connecting more than 1 input/output to the same output/input.