What material can I use between the MAX30105-based sensor and the external environment?
Plexiglas 7N, Gorilla 4 and 5 have been successfully used. As long as the spectral response is above 90%, then the material will not hinder proper operation of the MAX30105.