Can you please explain the meaning of the "Maximum Pass Voltage" specification listed in the datasheet for the ADG324x bus switches?
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
ADG3247
Production
The ADG3247 is a 2.5 V or 3.3 V 16-bit, 2-port digital switch. It is designed on Analog Devices’ low voltage CMOS process, which provides low power dissipation...
Datasheet
ADG3247 on Analog.com
ADG3249
Obsolete
The ADG3249 is a 2.5 V or 3.3 V, high performance 2:1 multiplexer/demultiplexer bus switch. It is designed on a low voltage
CMOS process, which provides...
Datasheet
ADG3249 on Analog.com
ADG3242
Production
The ADG3242 is a 2.5 V or 3.3 V, 2-bit, 2-port common-control digital switch. It is designed on a low voltage CMOS process, which provides low power dissipation...
Datasheet
ADG3242 on Analog.com
ADG3246
Production
The ADG3246 is a 2.5 V or 3.3 V, 10-bit, 2-port digital switch.
It is designed on Analog Devices’ low voltage CMOS process,
which provides low power...
Datasheet
ADG3246 on Analog.com
ADG3241
Production
The ADG3241 is a 2.5 V or 3.3 V, single digital switch. It is
designed on a low voltage CMOS process, which provides low
power dissipation yet gives high...
Datasheet
ADG3241 on Analog.com
ADG3245
Production
The ADG3245 is a 2.5 V or 3.3 V, 8-bit, 2-port digital switch.
It is designed on Analog Devices’ low voltage CMOS process,
which provides low power dissipation...
Datasheet
ADG3245 on Analog.com
ADG3243
Production
The ADG3243 is a 2.5 V or 3.3 V, 2-bit, 2-port digital switch with individual channel control. It is designed on a low voltage CMOS process, which provides...
Datasheet
ADG3243 on Analog.com
ADG3248
Production
The ADG3248 is a 2.5 V or 3.3 V, high performance 2:1 multiplexer/demultiplexer. It is designed on a low voltage CMOS process, which provides low power...
Datasheet
ADG3248 on Analog.com
Can you please explain the meaning of the "Maximum Pass Voltage" specification listed in the datasheet for the ADG324x bus switches?
The maximum pass voltage specification on the ADG324x family of bus switches represents the maximum voltage that can be passed though the device with some attenuation due to the ON resistance of the channel depending on the load current.
If the signal applied to the switch pins (for example A) exceeds this value, the output voltage (at pin B) will be clamped to the maximum pass voltage value.
This specification is only valid when the bus switch is in the ON state and applies to both switch pins (when the voltage applied to pin A exceeds the specification, the voltage on pin B gets clamped and vice versa).
Hi ,
Could you please let me know if the Vp specification is going to change along with the change in VCC .
Vp Spec specifies only at a particular Vcc if so then most of the devices with 1.8 has a margin of +/- 0.3V.
Please let me know if you have the details with regards to Max/Min for Max/Min VCC .
Thanking you
With best regards and wishes