Spice model for ADG1611 (quad SPST) ?

I'm thinking of using ADG1611 (quad SPST with low Ron of about 1 Ohm) in a design.

I could not find the Spice model for ADG1611 in the ADI_All_Spice_Models Spice bundle. However, I could locate the model for ADG1211 (another quad SPST with Ron ~= 120 Ohm) and tried it briefly as a poor man's substitute, only to find that the ADG1211 spice model appears being simulated with an Ron running into KOhms, which is higher than the ADG1211 spec itself. So even the dc transfer function would be pretty inaccurate (apart from the capacitances being different which I could have lived with).

Can I get a Spice model for ADG1611 ?

Thanks

  • 0
    •  Analog Employees 
    on Oct 25, 2011 4:45 PM

    Hi,

    Unfortunately we do not have a spice model available for the ADG1611 at this time.

    What supplies are you using for the ADG1611 model?If the ADG1211 model is simulated with a dual 5V supply the model will not function properly. The ADG1211 is optimized for +/-15V operation.

    You could try using +/-15V supplies for the ADG1211 or alternatively, If you are operating the part at 5V single supply you could try the ADG711 or ADG811.

    What is the application?

    Regards,


    Michael

  • Thanks, Michael. In my model, the ADG1211 (which is a substitute) has a single supply of +12V. This matches one of the specified modes of operation (page 5 of spec). I'm seeing about 1K of Ron in this setting.

    I want to use the ADG1611 in the real circuit. It will be used to set the gain for an AD8221 IN-Amp (also single supplied with +12V). ADG1611's low Ron improves gain accuracy and linearity as well as allows lower Rg's to be attained (for high gain). I have searched high and low but do not find any better part than ADG1611 for this application.  Thanks

  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:28 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin