Post Go back to editing

ADG608 or similar for +- 3.3V dual supply ?

Hello Everyone,

I've got signals oscillating between +35 mV and -35 mV and I need an analogue multiplexer to select from them. Signals are below 150 Hz. Supply to the circuit is dual supply 3.3V. What analogue multiplexer should I use ? I found ADG608 to be ok but I'm not sure if it's the most suitable and I'm not sure if it will work with dual supply 3.3V.

Thanks