Post Go back to editing

ADG888: Decoupling audio ground from power GND

Dear all,

the following schematic is for processing signals from/to different audio sources.

It uses a couple of ADG888 for the audio switching function, and a simple debouncer (MAX6816) to have a better control.

The question: is it better to keep the audio ground line separated from the main power supply GND ? Or is it mandatory?

Thank you for your idea!

M

audioswitch2.pdf
Parents
  • Hello Massimo,

    You will need to level shift the signals to pass them through the ADG888. Depending on the signal range will determine how much shifting you will require.

    We do have the ADG4613 which has negative signal passing capability. This can be configured to act like the ADG888 by tying D1 and D2 together and IN1 and IN2 together. Similarly, D3, D4 and IN3, IN4 will create the second SPDT.

    Regards,

    Sean

Reply
  • Hello Massimo,

    You will need to level shift the signals to pass them through the ADG888. Depending on the signal range will determine how much shifting you will require.

    We do have the ADG4613 which has negative signal passing capability. This can be configured to act like the ADG888 by tying D1 and D2 together and IN1 and IN2 together. Similarly, D3, D4 and IN3, IN4 will create the second SPDT.

    Regards,

    Sean

Children
No Data