Post Go back to editing

ADG888: Decoupling audio ground from power GND

Dear all,

the following schematic is for processing signals from/to different audio sources.

It uses a couple of ADG888 for the audio switching function, and a simple debouncer (MAX6816) to have a better control.

The question: is it better to keep the audio ground line separated from the main power supply GND ? Or is it mandatory?

Thank you for your idea!

M

audioswitch2.pdf
Parents
  • Hi Sean,

    many thanks for having driven my attention on this point. Everything is clear now.

    Considering that I want continue to use ADG888 for the project (USB for single power supply requirements are mandatory), can you help me on correcting the schematic in order to allow to bipolar signals to be processed correctly?

    I guess that at least a level shifting to Vcc/2 (= 2.5V) are necessary for each input, is it not?

    Can you suggest a single-chip solution based on AD?

    Many thanks for your help, it is really appreciated!

    Regards,

    Max

Reply
  • Hi Sean,

    many thanks for having driven my attention on this point. Everything is clear now.

    Considering that I want continue to use ADG888 for the project (USB for single power supply requirements are mandatory), can you help me on correcting the schematic in order to allow to bipolar signals to be processed correctly?

    I guess that at least a level shifting to Vcc/2 (= 2.5V) are necessary for each input, is it not?

    Can you suggest a single-chip solution based on AD?

    Many thanks for your help, it is really appreciated!

    Regards,

    Max

Children
No Data