Hello,
I need to switch different signals to an ADC. I already choose the AD7195 for my application.
In the application I need to multiplex a differential input of the ADC (channel AIN1 and AIN2).
I want to use a CMOS switch for that.
Another point is that I have an embedded system supplied by around 12V (9V to 20V in fact).
ADG1434 sound good for my application, but can I supply this part with my supply voltage (9V to 20V)?
Or is a regulated 12V mandatory?
In fact it is not plane to use differential +-5V or +- 15V on the board.