higher dual voltage on ADG759

Dear analog engineers,

I want to use the ADG759 for muxing my sensor signals at 40MHz.

The problem I have, is that the only voltages I have on my PCB are ±3,3V and ±5,5V dual suppllies.

I need the low Ron resistance, so other options are not available at Analog.

The absoluut maximum of the ADG759 is 7V (VDD to VSS), can I use the ADG759 on a

± 3,3V power supply without degrading the specifications???

Hopefully one of you can help me.

With kind regards,

Andre

Message was edited by: Andre Dekker Reply button does''nt work so I do it this way. The transition times of the two parts are way to low. I need to switch with 40MHz so is there any other option???

ADG759MUX.pdf
Parents Reply Children
No Data