Post Go back to editing

If ADN4612 can both support 1.25G 2.5G and 10G ?

My boards use SFP and SFP + interfaces, wanted to support both 1G 2G 10G rate, if this can be support? what required for pcb layout,if have  schematic for reference。

when the rate is 2.5G it need ADN2812 CDR chip,and when the rate is 10G the CDR need bypass.Usually the CDR is at rx side,but needs to be compatible 10G,i used follow way. when the rate is 10G ,the signal flow is R1--T1,when the rate is 2.5G ,the signal flow is R1--T7--CDR--R7--T1.If this design is OK? The signal through ADN4612 will add jitter ,if this effect is large or small in the 2.5G rate?

Parents
  • Hi Fangquan,

    The ADN4612 is an asynchronous, protocol agnostic crosspoint switch, which means it can support any protocol (assuming NRZ modulated) and any data rate up to the maximum rating of 11.3Gbps.  1.25G, 2.5G 10.3G and many more are supported.  You can see from Figure 30 in the datashee that the residual jitter of the ADN4612 is fairly flat across the full range of supported data rates.

    Just curious.  Why does your application only require CDR at lower datarates (1.25G or 2.5G), but not at 10Gbps?

    You may also be interested in our new ADN2915, any rate continuous tuning CDR, that supports data rates from 0.006Gbps up to 11.3Gbps.

    I can send evaluation board schematics off-line.

    Dave

Reply
  • Hi Fangquan,

    The ADN4612 is an asynchronous, protocol agnostic crosspoint switch, which means it can support any protocol (assuming NRZ modulated) and any data rate up to the maximum rating of 11.3Gbps.  1.25G, 2.5G 10.3G and many more are supported.  You can see from Figure 30 in the datashee that the residual jitter of the ADN4612 is fairly flat across the full range of supported data rates.

    Just curious.  Why does your application only require CDR at lower datarates (1.25G or 2.5G), but not at 10Gbps?

    You may also be interested in our new ADN2915, any rate continuous tuning CDR, that supports data rates from 0.006Gbps up to 11.3Gbps.

    I can send evaluation board schematics off-line.

    Dave

Children
No Data