ADG5412 Supply Voltage

Can the ADG5412 be used with +/-5V supply rails?

The datasheet states +/-9V to +/-22V supply range. The device appears to function correctly but I am required to show proof of compliance with manufacturers datasheet for the application.

Parents
  • 0
    •  Analog Employees 
    on Aug 6, 2014 1:36 PM

    Hello Martin,

    To be clear, it is the internal threshold voltages that is at issue here. At VDD = 9V, the internal VCC generator is properly engaged and the input voltages are specified across all temperatures. At lower voltages, the digital input is required to be over driven to ensure that the switch reacts correctly at all temperatures.

    Regards,

    Sean

Reply
  • 0
    •  Analog Employees 
    on Aug 6, 2014 1:36 PM

    Hello Martin,

    To be clear, it is the internal threshold voltages that is at issue here. At VDD = 9V, the internal VCC generator is properly engaged and the input voltages are specified across all temperatures. At lower voltages, the digital input is required to be over driven to ensure that the switch reacts correctly at all temperatures.

    Regards,

    Sean

Children
No Data