Post Go back to editing

ADG508F Operating supply voltage

Thread Summary

The user encountered an issue with the ADG508F multiplexer where the channel opens between input and output at -10°C with ±4.5V supply voltage. The final answer suggests that ±4.5V is too low, as the device is specified for ±15V operation. The internal VCC generator requires a minimum VDD of 8V, and the digital logic should be driven to VDD to ensure proper operation at low temperatures. The user will consult with ADI's local region for further advice.
AI Generated Content

Dear all,

The trouble occurred in our product using ADG508F.

It is Open between input and output in low temperature. (About -10 degrees C) 

*I am still seeing the phenomenon only by one individual.

*We are applying +4.5V,-4.5V to Vdd,Vss.

Q1) Possibly, is supply voltage too low?

      Or is it failure of device?

Q2) In a data sheet, it seems that there is no operation supply voltage range spec.

      Please let me know the recommendation supply voltage range.

Best Regards,

DMN

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.