Hi,
I would like to use ADG413 in my application. My power supply is -4V/+4V.
Is it possible to use ADG413 in this power supply range (Vdd=4V and Vss=-4V) ?
Hi,
I would like to use ADG413 in my application. My power supply is -4V/+4V.
Is it possible to use ADG413 in this power supply range (Vdd=4V and Vss=-4V) ?
HI Maxime,
The ADG413 may work but we do not have any data to support it at these supplies.
My recommendation is the ADG1613, 4xSPST which can be operated with +4/-4V supplies.ADG1613 datasheet and product info | 1 Ω Typical On Resistance, ±5 V, +12 V, +5 V, and +3.3 V Quad SPST Switches | Analo…
Fig 6 in the datasheet will give indication of its Ron performance. It will sit between ±3V operation and ±5V operation.
Is this part suitable for your application?
Alternatively, the ADG513 is an option.
Rgds,
Theresa.