Post Go back to editing

ADG417 VL threshold

Thread Summary

The user asked for clarification on the logic input thresholds (VIH and VIL) for the ADG417 when VL is set to +VDD (e.g., +15V or +24V). The final answer provided a figure from an attached document showing the applicable thresholds for the ADG417, indicating that the thresholds vary with VL voltage. The user confirmed understanding the supply pin for logic but sought specific threshold levels for higher VL values, which were addressed in the provided figure.
AI Generated Content

Hello,

I'd like to clarify the threshold level of VL.  Since the data sheet says only at VL=5V, I'd like to know what the VL thresholds would be in case of VL=+VDD (ex. VL=+15V or +24V).  I think the VIH shouldn't be 2.4V at VL=+24V.

Could you tell me what the thresholds of VIL and VIH at VL=+VDD (greater than +5V) is ?

Thank you,

Regards,

Hiroshi