Post Go back to editing

ADG441 Implementation

Thread Summary

The user is troubleshooting an ADG441 setup where the signal at D1 does not change with the logic input at IN1. The final answer suggests checking the pull-up or pull-down resistors on the logic input and testing with a DC signal at S1, noting that a low logic input should keep the switch on.
AI Generated Content

I am having trouble getting the ADG441 to work properly and want to confirm that my setup is correct. To test the chip, I made the following connections:

analog ground/0v to GND

-9v to Vss

+9v to Vdd

0.5v 1KHz sine wave to S1

Logic input of 0v or 5v to IN1

No matter if I give IN1 0v or 5v, the signal received at D1 is always the same signal connected to S1. What am I doing wrong in my setup that is preventing the switch from opening?  

  • Hi Jody,

    Are you using pull up or pull down resistors on the logic input?  It would be worth changing the resistor value if you are.  Note for the ADG441, when the logic is low the SPST switch should be on.  Also worth testing using a  DC signal at first on S1 as the simplest use case. 

    Regards,

    Eric.


Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.