Post Go back to editing

AD5111 Writing issue

Thread Summary

The user is experiencing issues writing to the EEPROM of the AD5111 digital potentiometer when using a HIGH-LOW-HIGH-LOW cycle on the U/D# pin. The final answer indicates that EEPROM programming requires a positive pulse (LOW-HIGH-LOW) and the U/D line should be changed while CLK is LOW. The user should use the LOW-HIGH-LOW method for EEPROM programming.
AI Generated Content

Hello,

One of my customers is using the AD5111 digital potenziometer.

He has an issue with writing to his egisters

Their tining is according to the figure 3 in the data sheet

The CS is tied to "low" by pull down. During this cycle the CLK is in HIGH

The writing cycle is failed whther they start the U/D# pin from "HIGH" as follows: HIGH-LOW-HIGH-LOW - then the EEPROM programm is not succeeds.

Using the following U/D# cycle the EEPROM programm is performed successfully: LOW-HIGH-LOW .

I can't see any limitations for it in data sheet.

Do you have any idea why during the HIGH-LOW-HIGH-LOW cycle the writing to the eeprom is failed?

Thanks

Meir

Parents
  • Hi Meir,

    The EEPROM will only be stored on a positive pulse. LOW-HIGH-LOW

    Other than the EEPROM command, the datasheet states that the U/D line should be changed while CLK is LOW (see the basic operation section of the datasheet)

    Please advise the customer to have their U/D line LOW before attempting to program the EEPROM.

    Or in other words, use the LOW-HIGH-LOW method.

    Kind Regards,

    David

Reply
  • Hi Meir,

    The EEPROM will only be stored on a positive pulse. LOW-HIGH-LOW

    Other than the EEPROM command, the datasheet states that the U/D line should be changed while CLK is LOW (see the basic operation section of the datasheet)

    Please advise the customer to have their U/D line LOW before attempting to program the EEPROM.

    Or in other words, use the LOW-HIGH-LOW method.

    Kind Regards,

    David

Children
No Data