Post Go back to editing

ADG701/702 710L/702L as low current road switch

Hi All,

One of my customer wants low Iq road switch.

The Iq of ADP198 is 2.5uA typ/ 20uA max and is too large for his application.

The road current for his application is 10mA or less.

His supply voltage is 5.5V.

Then I will propose ADG701/702 or ADG701L/702L instead of ADP198.

I would like to double check with you that ADG701/702, ADG701L/702L can be used as low road current road switch.

Is there any precautions needed in this application?

Best Regards,

Ricky