hi
I have doubt regarding the maximum potential difference between DVCC and AVEE. As in Datasheet it is given 6V and in user manual it is shown that it takes AVCC=+5V, AVEE= -5V & DVCC = +5V. As per user mannual the maximum potential difference between DVCC and AVEE is 10V which contradict with the Datasheet. can anyone please clarify this.
From datasheet absolute maximum rating
1. AVCC - AVEE <= 11V
2. AVCC - DVCC <= 0.5V
3. AGND - DGND <= 0.5V
then How DVCC - AVEE <= 6V.
regards
Gautam