Post Go back to editing

ADV3202 - cropped video signals

Hello everybody,

 

I have a problem using the ADV3202. All output video signals are cropped at about 900 mV in a manner, that no sync is transmitted. VPOS is connected to +5 V, VNEG is connected to GND, VREF is supplied with 2.5 V and VCLAMP is connected to GND as well. (I tried several connections for VCLAMP and VREF, but neither worked)

 

Attached I have a snippet of the schematic and a sample of input and output video signal.

 

Can you please give me a hint to solve this problem? Thanks in advance.

0003_VOUT_ERROR.zip
Parents
  • Hi Anna,

    sorry, I forgot to mention, that I already replaced them with 0R. The video signal before was no video signal at all ...

    One more thing: All activated outputs have these 900mV level, even when there's no video signal applied or routed. All deactivated outputs are constantly tied to GND. Changing bit 193 didn't change anything.

    Regards,

    Daniel

Reply
  • Hi Anna,

    sorry, I forgot to mention, that I already replaced them with 0R. The video signal before was no video signal at all ...

    One more thing: All activated outputs have these 900mV level, even when there's no video signal applied or routed. All deactivated outputs are constantly tied to GND. Changing bit 193 didn't change anything.

    Regards,

    Daniel

Children
No Data