Hello,
Is there data avalible of the Harmonic Distortion ADV3221.
In the datasheet there is a graphic of the ADV3222 (figurer 49) not the ADV3221.
The frecuency of interest is 100KHz..10MHz.
Thanks in advance,
Ronald Dekker
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. | Open | |
ADV3221
Production
The ADV3221 and ADV3222 are high speed, high slew rate, buffered 4:1 analog multiplexers. They offer a −3 dB signal bandwidth greater than 800 MHz and...
Datasheet
ADV3221 on Analog.com
ADV3222
Production
The ADV3221 and ADV3222 are high speed, high slew rate, buffered 4:1 analog multiplexers. They offer a −3 dB signal bandwidth greater than 800 MHz and...
Datasheet
ADV3222 on Analog.com
Hello,
Is there data avalible of the Harmonic Distortion ADV3221.
In the datasheet there is a graphic of the ADV3222 (figurer 49) not the ADV3221.
The frecuency of interest is 100KHz..10MHz.
Thanks in advance,
Ronald Dekker
Hi, Ronald.
Regardless of gain, the harmonic distortion is still the same. It might reduce about 1dBc and that is just negligible. ADV3221 and ADV3222 woud have the same plot as long as the test setup of harmonic distortion is the same (ex. Vout=1Vpp for both gain 1 and 2).
Harmonic distortion would increase as the frequency increases. When your output also reached the rails or near the rail then the distortion would also increase.
I can't provide you the plot of the ADV3221 but basically they would almost be the same.
Regards,
Anna
Hello Anna,
Thanks for your answer so far.
Can you give me a indication what the harmonic distrortion is below 10MHz. Let say at 1MHz.
Best regards,
Ronald Dekker
Hi, Ronald.
We will try to measure the distortion of ADV3221 at lower frequencies (below 10MHz) but we suspect that it will be worse than the ADV3222 because distortion degrades with heavier loads (50ohms).
For the meantime, can you please share your application? If it's okay please also share your schematic or at least a block diagram. Another question, will you use 50ohm load?
Regards,
Anna