Post Go back to editing

ADG5421

hello,

my system includes fpga and power supply that are not related and their gnd isn't common

as I described in the attached schem.

I want to switch the power supply 28v output

how should I connect the gnd?

thank you

Parents
  • Hi,

    Do you mean you have both a Digital and Analog ground on the same PCB which are connected together at a certain point on the PCB? If that is the case then you would want to connect the switch to the power supply ground as the FPGA ground would be quite noisy.

    If the GNDs are completely unrelated to each other then that could create different issues altogether. You would have to ensure that digital logic voltages met the VIL and VIH limits in respect to the switch power supply GND and that it does not exceed the absolute max ratings of the part. This would be difficult if there is no relationship between the two GNDs.

    Regards,

    Stephen

Reply
  • Hi,

    Do you mean you have both a Digital and Analog ground on the same PCB which are connected together at a certain point on the PCB? If that is the case then you would want to connect the switch to the power supply ground as the FPGA ground would be quite noisy.

    If the GNDs are completely unrelated to each other then that could create different issues altogether. You would have to ensure that digital logic voltages met the VIL and VIH limits in respect to the switch power supply GND and that it does not exceed the absolute max ratings of the part. This would be difficult if there is no relationship between the two GNDs.

    Regards,

    Stephen

Children
No Data