Post Go back to editing

Analog Switch for RS232 Level.

Hi everyone,

I need to work on an analog switch which will switch the RS232 (+/- 10VDC) signal from different RS232 serial communication.

I tried ADG333 with MAX232IDR, but it will draw too much current when RS232 is in Mark (-8.9VDC), then it will pull it to -0.89VDC.

Does everyone how to make analog switch for RS232 signals?

Thanks for help.

Parents
  • Hi KRZ,

    Since I use a single power supply of +5VDC to MAX232, and +12VDC for ADG333(it was +5VDC incorrect on the schematics.

    when TTL is 0 (0VDC-Ground), RS232 Level is +8.57VDC, the ADG on COM is +8.57VDC, then NC/NO works as expected,

    However When TTL is 1 (+5VDC), if no connected to ADG333 on COM, RS232 Level will be -8.57VDC(negative). but once I connect it to ADG333 on COM, it drops to -0.67V, it did not stay -8.57VDC, and draw 0.02mA. What went wrong with TTL Logic Truth (1)?

    Please review this part of schematics. Thanks

Reply
  • Hi KRZ,

    Since I use a single power supply of +5VDC to MAX232, and +12VDC for ADG333(it was +5VDC incorrect on the schematics.

    when TTL is 0 (0VDC-Ground), RS232 Level is +8.57VDC, the ADG on COM is +8.57VDC, then NC/NO works as expected,

    However When TTL is 1 (+5VDC), if no connected to ADG333 on COM, RS232 Level will be -8.57VDC(negative). but once I connect it to ADG333 on COM, it drops to -0.67V, it did not stay -8.57VDC, and draw 0.02mA. What went wrong with TTL Logic Truth (1)?

    Please review this part of schematics. Thanks

Children
No Data