Hello all,
I think you all know the famous channel protection devices from AD. Starting with the AD467 / ADG465, and followed by the ADG5462F.
All of the have two common attributes:
- they are fantastic devices
- they come in quite huge packages
I wonder if it is possible to build some kind of 4 channel ADG467 in a UDFN10 package.
The UDFN10 package is common for TVS diode arrays. It allows a nice pass-through pinout and is only 2.5 x 1.0 mm. This would be really cool stuff.
Do you agree?
I am looking forward to your answers.
Regards, Niels