Post Go back to editing

ADG858 for USB?

Thread Summary

The user inquired about using two channels of the ADG858 for USB data lines, despite the lack of USB-specific testing in its datasheet. The support engineer recommended the ADG774 or ADG772, which are 12Mbps switching compliant and better suited for USB applications. The user opted for two ADG772 devices due to package size constraints.
AI Generated Content

Hi,

Could you please confirm if I can use two channels of ADG858 for USB data lines? I checked the important specifications (like On resistance, on resistance flatness, matched on resistance, bandwidth) for this device and compared with some devices which are recommended by AD for USB applications, such as ADG787. It seems that the USB requirements are satisfied by ADG858 too. But there is nothing mentioned about USB in ADG858's data sheet. I didn't find an eye diagram in it either.

The reason that I prefer to use ADG858 is that I need its four matched channels and I will be using two of them for USB data lines. Could anyone tell me if I am going wrong about this?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.