Post Go back to editing

AD8192  application issue

Usually AD8192 is used  for two HDMI input and one HDMI output .

Can I swap the signal direction, used for one HDMI input and two HDMI output.

  • Hi,

    The AD8192 data path is uni-directional and not bi-directional. Therefore, it cannot support the proposed configuration of driving a signal on one input and fanning it out to two outputs.

    ADI does provide network switches like the AD8159 that can support the desired configuration you are looking for. It provides the capability to fan-out the High-speed TMDS signals of the HDMI protocol, but it cannot support the fan out of the low-speed DDC signals.

    Regards,

    Jarrod