Post Go back to editing

AD8156 and ADN4612 in HDMI application

Can I use AD8156 and ADN4612 in HDMI 2.0 applications. They want to know whether these switches will work with HDMI 2.0 protocol. Thread 36599 on ADI’s Engineer Zone states “The ADN4612 is an asynchronous, protocol agnostic crosspoint switch, which means it can support any protocol (assuming NRZ modulated)”.

I have searched and cannot tell whether HDMI is NRZ modulated. Can you please confirm whether AD8156 and ADN4612 can natively switch HDMI 2.0.

Thanks,

  • Hi,

    Both the ADN4612 and AD8156 will support the HDMI 2.0 TMDS data rates of 6.0Gbps. HDMI is NRZ modulated. The asynchrnonous data path in both products is protocol agnostic and supports NRZ modulated signals from DC to the maximum data rate specified.

    Regards,

    Jarrod

  • Hi Jarod,

    As a follow-up to the above question, what circuitry would you advise to actually interface the HDMI inputs and HDMI outputs to the crosspoint switch since the electrical characteristics are not the same?  Or is there a way to configure the crosspoint to be compatible with the TMDS?

    Thanks

  • Hi,

    The ADN4612 VTTI and VTTO supplies operate at 1.8V and 2.5V respectively and therefore they must be AC-coupled to be compatible with HDMI interfaces. AC-coupling is acceptable in the HDMI standard as long as the HDMI receiver or HDMI transmitter provide a 50-ohm single-ended or 100-ohm differential termination to the 3.3V supply.

    Regards,

    Jarrod