Can i use AVDD =5V0,AVSS=0, in ADG2128?


Hi,

In my application i am using ADG2128, can i give vdd=5v0 and vss=0.

In datasheet there is only two option 12v0 single supply and +-5v0 dual supply,

Instead of 12v0 if we give 5V0 whats the difference?

Thankyou,

Sony Sunny.

  • 0
    •  Analog Employees 
    on Jul 21, 2016 7:06 PM

    Hi Sony,

    Yes, you can use the ADG2128 with Vdd=5V and Vss=0V and VL=5V. Please be reminded that VL sets the logic power supply of the part so it is necessary to retain it at 5V to ensure that the part would still perform as expected.

    There will be changes in the values of parameters of the device that we cannot guarantee. Please be reminded that we only guarantee specs tested and stated in the datasheet. Also, analog inputs would be limited since the part will be operating at +5V single supply only.

    Best Regards,

    May