Post Go back to editing

I have got a question about the ADG426 multiplexer

Thread Summary

The user inquired about connecting multiple ADG426 multiplexers with common WR and RS signals, given that the latch and all channels open functions are not required. The support engineer confirmed that this is feasible, advising to follow Table 9 in the datasheet for configuration.
AI Generated Content

Hi,

sorry for asking so much...

Can I connect several multiplexer with the same WR and RS signals if these functions are not needed?

For example I put WR=0 and RS=1, so I can switch all multiplexer by choosing the right select lines.

I do not need the 'latch function' and the 'all channels open' function .

However I have chosen this multiplexer because of the package.

Thanks!

Parents Reply Children
No Data