Post Go back to editing

ADG751 Source isolation

Thread Summary

The user inquires about using ADG751 CMOS switches with floating sources and high-speed gate driving. The final answer confirms that the input voltage must stay within -0.3V to VDD + 0.3V relative to the device GND, and the logic input must be 2.4V above GND to turn the switch on. A bootstrap circuit or isolation may be necessary to ensure these conditions are met.
AI Generated Content

Hello, 

I want to use ADG751 switches for a circuit I am working on. My switches in this circuit are floating (sources are not grounded), will be this a problem using ADG751 CMOS switches? Also, I am driving the gate(switch on and off in high speed around 1MHz) using a microcontroller, do I need to have an isolation for the floating source?  or I need a bootstrap circuit to ensure turning the switches on & off ?

Thanks

Jacob

  • Hi Jacob,

    The signal presented to the source/drain of the ADG751 needs to be between -0.3V and VDD + 0.3V so that the absolute max ratings are not violated. The absolute max ratings are referenced to the GND of the device so if the voltage source is floating you would need to be able to guarantee that the input voltage max range is not violated.

    The digital logic input high and input low voltages are also referenced to the GND of the device so the logic input signal needs to be 2.4V above the device GND for the switch to turn on.

    Regards,

    Stephen

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.