ADG1402B to support 1Amps

Hi All,

my requirement for switching DC Voltage upto 48V or 24V

maximum current is 1Amps

when i see this ADG1402B chip , it can support upto 430mA. so im thinking to combine two chips and rise the current range upto 850mA. is it possible?  or please provide me the CMOS switch which can afford current range upto 1A.

Thanks,

Ashok