What should I do with these Vcc and Vee pins? They are there for the output amplifier of the AD8113. Can I leave these disconnected when I'm using the AD8112? And where is the AVcc for output 7? It's not shown in the datasheet in figure 6.
AD8112
Production
The AD8112 is a low cost, fully buffered crosspoint switch matrix that operates on ±12 V for audio applications and ±5 V for video applications. It offers...
Datasheet
AD8112 on Analog.com
AD8113
Production
The AD8113 is a fully buffered crosspoint switch matrix that operates on ±12V for Audio applications and ±5V for Video applications. It offers a -3dB signal...
Datasheet
AD8113 on Analog.com
What should I do with these Vcc and Vee pins? They are there for the output amplifier of the AD8113. Can I leave these disconnected when I'm using the AD8112? And where is the AVcc for output 7? It's not shown in the datasheet in figure 6.
Hi.
Using AD8112, the AVcc pins 21, 22, 26, 30, 34, and 55 must be connected to +5V because these positive supply pins are for the inputs and switch matrix. The AVee pins 20, 24, 28, 32, 36, and 56 must be connected to -5V because these are negative supply pins for the inputs and switch matrix.
Looking at the datasheet of AD8113, the AVcc pin of OUT07 is pin 38. This should also be the same with AD8112 for I think they use the same die. I'll confirm this and will let you know.
To make sure that you power all the internal circuitry of the AD8112 or AD8113, connect all AVcc to the positive supply, the AVee to negative supply and the Agnd to ground.
Thanks.