Post Go back to editing

searching better leakage current than ADG701

Thread Summary

The user is seeking a replacement for the ADG701 with better or equal leakage current and multiple switches in a single package for use in a photodiode TIA. The ADG711 is recommended as it has a typical leakage current of 10pA and a maximum of 200pA, with low on resistance (2.5 ohms at 5V). The ADG701's leakage current min/max specs are not available, but the ADG711 is a quad SPST switch suitable for the application.
AI Generated Content

Hello,

I am searching for a replacement for the ADG701.
There are two relevant points:

1.) Better or equal leakage current.

2.) More than one switch in the package.

It will be used switching gain resistors in a photodiode TIA. See the picture!

I need a flat on resistance which wont disturb the lower 100k and a low leakage for the 10M resistor.

I have done tests with the ADG701 and we are not allowed to get worse with leakage!

I assume that we have some problems with leakage temp drift, so I need a better part.

The ADG701 datasheet has only typical 10pA, but says nothing about min/max oder full temp.

You have several switches which are equal to typ 10pA, but these devices show relatively large currents in the min/max or full temp statement.

I would like to have 2, 3 or 4 switches in one case. So I found the ADG711.

Please tell me, is the leakage better, worse or equall?

I have red that all leakage comes from the ESD diodes on source and drain.
So I assume, that devices made for lower currents have smaller diodes and therefore have lower leakage currents.

True?

Getting better leakage values is more important than the number of switches in one package!

Thanks a lot!

Regards, Kai Toennies

Parents
  • Hi Kai,

    The ADG701 was first released way back 1998 and the min and max specs were not characterized before. So unfortunately, the data you are asking for is not available.

    The ADG711 on the other hand, has leakage current min and max specs as low as 10pA typ and up to 200pA and is more suitable for your application requirement: equal leakage current and more than one switch in a package. The ADG711 is also a quad SPST switch with low Ron = 2.5 ohms at 5V supply and is available in 16 ld SOIC and 16 ld TSSOP package.

    Let me know if this helps.

    Best Regards,

    May

Reply
  • Hi Kai,

    The ADG701 was first released way back 1998 and the min and max specs were not characterized before. So unfortunately, the data you are asking for is not available.

    The ADG711 on the other hand, has leakage current min and max specs as low as 10pA typ and up to 200pA and is more suitable for your application requirement: equal leakage current and more than one switch in a package. The ADG711 is also a quad SPST switch with low Ron = 2.5 ohms at 5V supply and is available in 16 ld SOIC and 16 ld TSSOP package.

    Let me know if this helps.

    Best Regards,

    May

Children
No Data