Post Go back to editing

searching better leakage current than ADG701

Thread Summary

The user is seeking a replacement for the ADG701 with better or equal leakage current and multiple switches in a single package for use in a photodiode TIA. The ADG711 is recommended as it has a typical leakage current of 10pA and a maximum of 200pA, with low on resistance (2.5 ohms at 5V). The ADG701's leakage current min/max specs are not available, but the ADG711 is a quad SPST switch suitable for the application.
AI Generated Content

Hello,

I am searching for a replacement for the ADG701.
There are two relevant points:

1.) Better or equal leakage current.

2.) More than one switch in the package.

It will be used switching gain resistors in a photodiode TIA. See the picture!

I need a flat on resistance which wont disturb the lower 100k and a low leakage for the 10M resistor.

I have done tests with the ADG701 and we are not allowed to get worse with leakage!

I assume that we have some problems with leakage temp drift, so I need a better part.

The ADG701 datasheet has only typical 10pA, but says nothing about min/max oder full temp.

You have several switches which are equal to typ 10pA, but these devices show relatively large currents in the min/max or full temp statement.

I would like to have 2, 3 or 4 switches in one case. So I found the ADG711.

Please tell me, is the leakage better, worse or equall?

I have red that all leakage comes from the ESD diodes on source and drain.
So I assume, that devices made for lower currents have smaller diodes and therefore have lower leakage currents.

True?

Getting better leakage values is more important than the number of switches in one package!

Thanks a lot!

Regards, Kai Toennies

Parents
  • Hi Kai Toennies,

    I'm confused, you mentioned 100k and 10M resistor above but looking at your schematic, I don't see any 100k and 10M? I can see 470k and 15M though. Please clarify.

     

    For ADG701 replacement, yes the ADG711 will be suitable for your application requirement: equal leakage current and more than one switch in a package. The ADG711 is a quad SPST switch with low Ron = 2.5 ohms at 5V supply, and has 10pA typ and up to 200pA max of leakage current only.

     

    For leakage, I would not say that it all came from the ESD diodes, it does contribute but leakage is mostly caused by the parasitic in the switch itself.

     

    Let me know if this help.

     

    Best Regards,

    May

Reply
  • Hi Kai Toennies,

    I'm confused, you mentioned 100k and 10M resistor above but looking at your schematic, I don't see any 100k and 10M? I can see 470k and 15M though. Please clarify.

     

    For ADG701 replacement, yes the ADG711 will be suitable for your application requirement: equal leakage current and more than one switch in a package. The ADG711 is a quad SPST switch with low Ron = 2.5 ohms at 5V supply, and has 10pA typ and up to 200pA max of leakage current only.

     

    For leakage, I would not say that it all came from the ESD diodes, it does contribute but leakage is mostly caused by the parasitic in the switch itself.

     

    Let me know if this help.

     

    Best Regards,

    May

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.