Post Go back to editing

The spice model for Multiplexer ADG608 and ADG658  have problem in PSPICE.Not compatible?

Thread Summary

The user encountered issues with the ADG608 and ADG658 spice models in PSpice, resulting in simulation errors. The final answer suggests checking the project file to ensure all libraries are properly imported. A known issue with the ADG608 model has been addressed with an updated version, and a new ADG609 model is in the works.
AI Generated Content

Spice model for Multiplexer ADG608 and ADG658 have problem in pspice simulation.(Orcad pspice 16.6 ),

I have  convert *.cir to *.lib and *.olb. It cannot get the right result.
The simulation even aborted for ADG608 (ERROR(ORPSIM-16144): Value may not be 0).

The same simulation circuit can get the right answer with SN74LV4051A model from other vendor.It is the

simplest channel selection test circuit.

So have the model for the two part be run in PSPICE?Or It have a  specific simulation software?

Parents Reply Children